Part Number: DS90UB933-Q1EVM
Other Parts Discussed in Thread: DS90UB934-Q1EVM, LM53601-Q1, LM2941
Hi,
Lately, I received from TI :
DS90UB933-Q1EVM and DS90UB934-Q1EVM for evaluation.
DS90UB933-Q1EVM user manual states that POC from DS90UB934-Q1EVM deserializer board should be (5V<=VPoC<=9V) .
Pls. see doc "SNLU210B–July 2016–Revised December 2017 " page 2.
DS90UB934-Q1EVM is has arrived from TI with jumpers that set POC_voltage to 9V.
However, when powering up DS90UB934-Q1EVM with external 12V , it delivers on POC voltage of 12V.
My question :
Is it safe to connect the two boards by coax although DS90UB934-Q1EVM delivers to DS90UB933-Q1EVM on POC 12V and not 9V ?
Thanks
DS90UB934-Q1EVM deserializer board for connection