I need to transmit and receive at the same time so I can verify the transmitted data is valid. The specification only indicates receiving when DE = 0 and RE = 0. I would like to have DE = 1 and RE = 0 so I can receive and transmit at the same time. Is this valid