Part Number: TLK10232
Hi team
Could you let me know your advice for following situation?
Customer's condition
1. TLK10232CTR is being used for 10 GB Ethernet to XAUI, but there is problem that seems to be caused by this IC.
2. In the communication IF using TLK1023, a 10GB Ethernet communication error occurs.
3. When send 5,000 to 6,000 PING commands, it detects about 5 to 50 communication errors.
4. An error occurs only Ach. No error is detected in Bch.
5. Error frequency is high at low temperature start (error about 50 times / 6,000 Ping), error frequency is low at high temperature start (about 5 errors / 6,000 Ping).
6. Even if the temperature changes after startup, there is no change in subsequent error frequency. The error frequency depends on the PHY temperature at startup.
7. Confirmed communication error with 2 out of 8 PHYs. The remaining 6 are normal.
8. Since the error frequency is caused by the PHY temperature at startup, it is specified that there is a factor in the PHY.
9. Confirmed that the XAUI communication waveform, power supply waveform, clock waveform (jitter) was not problem.
Customer's question
1. Is there any trouble similar to the above in the product? Does TLK10233 have any issue?
2. The error frequency depends on the temperature at startup. Does the IC calibrate at startup?
3. Please let me know if there are any design factors.
4. If you need schematic and waveform, I will send offline.
Best Regards,
Takanori Yuzawa