Part Number: DP83TC811SEVM
Other Parts Discussed in Thread: MSP430F5529, DP83TC811
Hi Team,
I'm doing a little project to understand the communication via automotive Ethernet PHY DP83TC811S and evaluate the DP83TC811S using DP83TC811SEVMs. About these I have the following questions:
1. I read the User's Guide of DP83TC811SEVM, in order to link 2 EVMs I need a MatENET cable assembly which is product of TE Connectivity. The first question is that I need to purchase this cable assembly or is it possible to get the cable from TI.
2. Now I have 2 EVMs, 2 MSP430F5529 Launchpads and USB 2 MDIO. I have read the documentations of these hardware and software. Using USB 2 MDIO the register of EVM can be read and written. so is it possible using them to implement some simple functions, such as using USB 2 MDIO to access the register of the EVM, one set of EVM and MSP430 as master, and the other set as slave, the master sends a massage via this Ethernet PHY to the slave to light an LED.
3. if the test above can not be achieved with these hardware and software, which hardware and software I need to implement the function like lighting an LED.
4. Is there any training material about the DP83TC811SEVM except User's Guide and Datasheet of DP83TC811S.
Best Regards,
Zhouyang Liu