Part Number: DP83620
I am looking at the MDIO/MDC interface to program the registers from FPGA, but the interface core is not ready yet.
wondering if no register configuration can work for 100BaseTX as default ? Firstly, try to work with TXCLK, TXEN, TXD[3:0] data between FPGA and DP83620 .
Will it work without an configuration through MDIO/MDC ?
the MAC Controller will send 32bit data format.. is there any data bit ordering to 4bit MII data format for DP83620?
Regards vrai