This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10232: May TLK10232 suit use bridge 10GKR to SFP application?

Part Number: TLK10232


Hi Sir 

My customer have Backplane Links project and need  12 sets 10GKR  transfer to 12 SFP signals. 

May we know TLK10232 suit this kind application? may we have related reference design can share to customer?

                                                                        Bogey

  • Hello,
    In general, the answer is yes. Please tell more about the application.
    Regards,
    Yaser
  • Hi Yaser

    there have some question need check with you.

    a. the line side line card, in Host side(HD side), may we know there need set to 10GBASE-KR or XFI? 

    b. Our line card SFP+ connector need SFI signal. therefore we need survey 10GBASE-KR to SFI or  XFI to SFI PHY(or Retimer)

    c. May we know what ti chip set solution use in this kind application?

                                         Bogey

  • Bogey,


    If I understand your request correctly, you would like to go from 10GBASE-KR or XFI [Host] to SFI [SFP+ connector]? TI does not have specific 10GBASE-KR to SFI or XFI to SFI devices but we have a re-timer that could work for this application, DS110DF111 as well as TLK10232.

    TLK10232 is a XAUI [Low Speed Side] to 10GBASE-KR/SFI/XFI [High Speed Side] with two channels, channel A and channel B. You could make an internal connection form channel one A to channel B using the internal data switch of TLK10232. This will allow you to connect the high speed sides of channel A and channel B to go from 10GBASE-KR to SFI. This will require configuring many of the internal registers as auto negotiation and link training must be disabled.