Part Number: DP83848T
Other Parts Discussed in Thread: AM3352
Tool/software: Linux
Hi Sir
We used AM3352 with DP83848T for design. And we would like to use Ethernet port for ping IP.
DP83848T is set as RMII mode and the connection between CPU and DP83848T is correct.
When we execute ping command and it always failed.
we have measured some signal and need your suggestion as below
a. we measure PFBOUT/ RBIAS pin and the voltage is 1.76V
b.RESET_N(Pin23) is 3.0V
c. RX_DV/MII_MODE (pin 39) pulled up to 3.3v --> configured as RMII mode
d. AVD33 (pin18), IOVDD33(pin1, 26) - 3.3v
e. X1 (pin 28) - 50 Mhz from osc
f. MDC (pin 25) - 1.0Mhz~1.9Mhz -> please help confirm this vfrequency is ok or not.
g. COL/PHYAD0(Pin35) -> we have pull up this pin to 3.3V using a 2.2K resistor .
At bootup status, this pin bring up from 0V to 3.3V sometimes. After entering system, the level of COL/PHYAD0 keep low.
please help to confirm the status is ok or not.
Thanks for your suggestion
BR
Yimin