Part Number: PCA9306
Hi, team.
I have any questions about PCA9306 from customer.
<Question>
1.Is the description of Figure 10 on Datasheet P13 correct?
Because, the explanation of the red line is "VDPUX≤2V", but the waveform line in the range of 2.0 to 5.5 V.
(Black line is the reverse)
2.To calculate the bus capacity, measure the rising waveform of SCL and SDA, is it calculating to use the formula "tr = t2 - t1 = 0.8473 × Rp × Cb" in the slva689 document ?
Example:When the rise time is 1us, the pull-up resistor is 10 kΩ.
"Cb = 1*10^-6 / (0.8473*10000) ≈ 118pF"
Best regards,
Masumi Sekiguchi