This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP139: Success higher resolution format

Part Number: SN75DP139

Hello,

The customer tried apply 2560x1440 DVI resolution data by using SN75DP139 then the image can be displayed.

DP75DP139 resolution max is defined as 1920x1200 @  60Hz so the above will exceed the spec.

I think  higher speed data is applied SN75DP139 and it succeed to transmit the data.

Do you think SN75DP139 can handle 2560x1440 DVI data?

Why can this format succeed to display? This is the customer question.

The configuration is below.

DDI_TX[3:0] -> SN75DP139RGZ IN_D[1:4] -> SN75DP139RGZ OUT_D[4:1] -> DIV-D connector

Best regards,

Toshihiro Watanabe