Part Number: TLK2711-SP
I am using the TLK2711-SP.
Unfortunately, I have an open-circuit track on one of the Tx differential tracks internal to my pcb, and would like to repair it instead of scrapping the board.
How practical is it to repair the board with an external wire link?
We have processes for the repair, it's getting the required performance afterwards is the issue.
How closely do I need to match the path lengths and impedances between the 2 differential tracks?
I am operating at 80 MHz clock, so a 1.6 Gbps raw data rate.
Many thanks
Michael