Part Number: DS90UB960-Q1
hello,
Dadtasheet says that when synchronized CSI2 forwarding is used the "Video arriving at input ports should be synchronized within approximately 1 video line period".
If you use Synchronized mode which sends the clock from 960 to 953, you can easily synchronize between multiple cameras because they operates at same clock domain.
If you use non-synchronize mode, is it possible to purely synchronize multiple cameras? the local oscillator at each cameras have part to part variation, so in short time cameras could be synchronized but in long time it seems there is a chance for not arriving the video data at input ports within 1 video line period. Is my assumption correct?
if correct, is it possible to use synchronized forwarding for non-sync mode?
please tell me whether Synchroized forwarding can be used with 913A//933 as well.