Part Number: PCA9306
Hi Team,
I got a question, from the datasheet PCA9306, in 6.5 section. it shows that it's on state when EN is 0.6V higher than VI (VI=2.4V, EN=3V & VI=1.7V, EN=2.3V)
While in 6.8 section. The test condition is EN=3.3V, VIH = 2.3V, which means EN is 1volt higher than VIH. my question is why VIH is 2.3V (according to the figure above, it's on-state when EN is 0.6V higher than VI, I guess VIH should at least be 2.7V)?
thanks a lot.
yang