Other Parts Discussed in Thread: TIDA-060017
I am trying to evaluate options for a back-plane interface ( order of 20-50Mbps or higher) with cost being a major driving factor. I seem to have narrowed down to either M-LVDS or RS485 (I've seen xcvrs in the 25Mbps range from TI, which may be also be OK). What I am looking for is:
1. A good reference design/application note or any data that shows this back plane design implementation?
2. Given that the speeds are 50Mbps, what would be the recommended link layer ? Any recommendations on the TI micro controllers that can be interfaced to these bus xcvrs? Are there any micro controllers supporting high speed serial interfaces (considering UARTs on existing uC may not be suitable)
Regards
R