Part Number: TCA9517
Hi team,
can TCA9517 use as buffer only? suppose to VCCA and VCCB connect to 3.3V that can implement buffer function according to d/s figure 9 typical series application.
BR,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9517
Hi team,
can TCA9517 use as buffer only? suppose to VCCA and VCCB connect to 3.3V that can implement buffer function according to d/s figure 9 typical series application.
BR,
SHH
Hey SHH,
Yes, you can use TCA9517 at VccA=VccB=3.3V. The thing you need to keep in mind when using buffers in series is to make sure the sides with static voltage offsets are not connected to each other. This means B side of TCA9517 cannot connect to another B side TCA9517. A to A and A to B is okay but not B to B.
Thanks,
-Bobby