Part Number: DS90UB953-Q1
Hi,
can somebody explain how to clear CRC_ERR, LINK_LOST_FLAG and BIST_CRC_ERR bits in the general status register. There are some inconsistencies in the document.
This is from the DS:
Back Channel CRC error detected
This bit is set when the back channel errors detected when BC LINK DET is asserted. This bit is cleared upon read of CRC_ERR_CLR register.
Now, CRC_ERR_CLR register does not exist. What exists is the CRC_ERR_CLR bit in the BC_CTRL register. However, this bit is described as:
3 CRC_ERR_CLR (R/W)/SC 0x0 Clear CRC error 0: Disable clear 1: Enable clear
So do I need to write this bit, read or what?
Similar is for the other two status bits mentioned above.
Thanks in advance,
Jura