This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: DP83867 PHY will not work with forced 1000F

Part Number: DP83867IS


I am working on custom HW.  The DP83867 PHY will auto-negotiate to 1000F, no problem.  However, when I attempt to force the link to 1000F, the link is never established.  I set the ethernet port to 1000F and no auto-negotiate, but this did not help. If I force 10F or 100F, the link is established.  I only have issues with 1000F.

I dumped the first 32 registers. Thank you for any help you can provide.

0x0000 --> 0x00000140
0x0001 --> 0x00007949
0x0002 --> 0x00002000
0x0003 --> 0x0000a231
0x0004 --> 0x000001e1
0x0005 --> 0x00000000
0x0006 --> 0x00000064
0x0007 --> 0x00002001
0x0008 --> 0x00000000
0x0009 --> 0x00000300
0x000a --> 0x00000000
0x000b --> 0x00000000
0x000c --> 0x00000000
0x000d --> 0x00000000
0x000e --> 0x00000000
0x000f --> 0x00003000
0x0010 --> 0x00005048
0x0011 --> 0x0000a802
0x0012 --> 0x00000000
0x0013 --> 0x00000040
0x0014 --> 0x00002fc7
0x0015 --> 0x00000000
0x0016 --> 0x00000000
0x0017 --> 0x00000040
0x0018 --> 0x00006b90
0x0019 --> 0x00000000
0x001a --> 0x00000002
0x001b --> 0x00000000
0x001c --> 0x00000000
0x001d --> 0x00000000
0x001e --> 0x00004202
0x001f --> 0x00000000