This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: DS90UB953/954 & DS90UB913/914 GPIO

Part Number: DS90UB953-Q1


Dear Sir,

Please refer below diagram,

The Camera would take "Flash or strobe output" signal connect to DS90UB953/913 GPIO do a input then GS90UB954/914 GPIO can to tigger IR LED Driver.

The signal is 1.8V square wave, 30~60Hz, duty arround 5~15%

Please you kindly review & provide suggestion.

Thanks!