This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: How much is the max throughput of DS90UB954?

Part Number: DS90UB954-Q1


Dear TI expert,

I want to transmit two 4K image sensor by two DS90UB953 to one DS90UB954, the total payload is 3840*2160*RAW10* 30Fps *2 Channel = 4,976,640,000= 5Gbps, which is lower than 6Gbps (1.5Gbs *4 lanes)

I want to confirm is it practicable for this case?

Thanks.