Part Number: DP83867IS
Hi team,
My customer is evaluating DP83867IS but they want to configure it to 100Mbps mode. I noticed that in the page 92 in our datasheet, the default connection is all the 4 pairs MDI lines are connected to RJ45. My question is if we configure it to 100Mbps mode instead of 1000Mbps mode, which 2 pairs are used and which 2 pairs are not used? The used or unused 2 pairs are fixed or can be software configured? Can we leave the unused pairs open? Thanks.
Best regards,
Wayne