This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD / TVS suggestion for +/- 8 kV ESD and automotive transients

Other Parts Discussed in Thread: TVS3300

Hi,

I would like help selecting ESD protection or TVS for a 40 V automotive LDO. The LDO needs external protection to pass +/- 8 kV ESD testing and automotive ISO7637-2 transient pulse 3b up to 100 V.

We will have a reverse protection diode and input cap on the LDO that should also help with the ISO7637-2 pulse 3b test. The LDO max recommended input voltage is 40 V, and abs max is between 42 V and 45 V.