Part Number: PCA9546A
Other Parts Discussed in Thread: PCA9548A
Hi Guys
Our customer is using our device for I2C level shifter. In our datasheet, Vpass:
"In order for the PCA9546A to act as a voltage translator, the Vpass voltage must be equal to or lower than the lowest bus voltage. For example, if the
main bus is running at 5 V and the downstream buses are 3.3 V and 2.7 V, Vpass must be equal to or below 2.7 V to effectively clamp the downstream bus voltages."
Why do we have to limit Vpass lower than lowest bus voltage?
What is it about the Internal detailed logic circuit?Could you explain why the Vpass is lower than lowest bus voltage?
Thanks
-Pengfei