Other Parts Discussed in Thread: SN65DSI83, DS90UB928Q-Q1, DS25BR100, DS25BR440, SN65LVDS93A
Hi, I would like to connect a small TFT display that uses LVDS, 4 channels for data and 1 channel for clock. Data rate is maximum 200 Mbps per lane. Very strict EMC requirements are applicable, namely automotive. What would be the maximum length of a typical LVDS cable that would still work in this environment? Length could be up to 1 meter. I am wondering from what length onwards I should use something like FPD Link III SerDes (e.g. DS90UB927)? Or would that be overkill? BOM cost is important.
Update: the device driving the LVDS signals is TI SN65DSI83.