Part Number: SN65DSI84
Hi Team
I have a question about SN65DSI84.
As a device, you can confirm that the MIPI input operates normally with LVDS output and that the image is being transmitted normally.
The PLL_UNLOCK bit of 0xE5 is "1".
Although it is stated that it can be cleared by writing 0xFF (RW1C), it does not become clear "0".
What kind of things can be considered?
When 0xE1[PLL_UNLOCK_EN] is "0", does 0xE5[PLL_UNLOCK] become invalid?
When 0xE1[PLL_UNLOCK_EN] is "0", does 0xE5[PLL_UNLOCK] become "1"?
Best Regards,
Ishiwata