This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: Tusb320 Application Question? How to control the outside when the following circuit is recognized by CC1 CC2 of Tusb320 to OTG function or earphone? Is there any problem with the circuit diagram?

Expert 2630 points
Part Number: TUSB320


Tusb320 Application Question? How to control the outside when the following circuit is recognized by CC1 CC2 of Tusb320 to OTG function or earphone? Is there any problem with the circuit diagram? 

Tusb320 Application Question?
How to control the outside when the following circuit is recognized by CC1 CC2 of Tusb320 to OTG function or earphone? Is there any problem with the circuit diagram?
How does Tusb320 recognize OTG function through CC1 CC2 and how does it control it?
How does Tusb320 control the sound of the external speaker when it recognizes the headset (audio output) function through CC1 CC2?
How to Control I2C Interface of Tusb320