This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD12S016: used as source or receiver -- does it make any difference ?

Expert 7280 points

Part Number: TPD12S016

Dear team,

My customer plans on having an end-equipment featuring both a HDMI input and an HDMI output.

Does it make any difference for the TPD12S016 ? I don't see why it would since the I2C is bidirectional. The only unused feature in case of receiver is the 5V load switch.

Please let me know if I miss something here.

Thanks a lot!

Best regards,

PA

  • PA,

    You are correct that the part will function correctly as either an input or an output as long as the load switch is bypassed for the input case.

    Also make sure your customer connects the port side connections to the port so the ESD functions correctly.

    Please click this customer thinks resolved button if I have fully answered your question or feel free to ask any further questions you have.

    Regards,
    Chuck