Part Number: TCAN1042V-Q1
Other Parts Discussed in Thread: TCAN1042-Q1
Hi,
My customer is using TCAN1042V-Q1, they are having below configuration questions:
1. general output port of the CAN interface have to used common mode choke, is TCAN1042 using choke-less structure?
2. will it become a EMI source if there are no choke at the output port of the CAN bus? is there an EMI filter reference circuit can used for reserve?
3. Can TCAN1042V-Q1 are able to meet transmission rate up to 2Mbits/sec?
4. if using 5V for supply voltage, can VIO pin been left floating or it needs to be connect to 5V?
Thanks for your help.