Part Number: SN65LVCP114
Can unused high speed inputs be left floating, or should they be biased? Design using 3 of the 4 inputs.
Blog note "Trouble passing 12G SDI" says inputs are biased to VCC-0.3 nominally.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVCP114
Can unused high speed inputs be left floating, or should they be biased? Design using 3 of the 4 inputs.
Blog note "Trouble passing 12G SDI" says inputs are biased to VCC-0.3 nominally.
Thank you. Do I need to bias both unused IN+ and IN-? I see industry and vendor differences whether IN- biasing is needed in addition to IN+.
I would recommend to bias only one input to Vcc . The internal bias to Vcc-0.3 will create a voltage across the input pair
Regards,
Lee