Part Number: SN65DP159
Other Parts Discussed in Thread: TMDS171
Hello.
We are considering TPS65DP159.
We are currently verifying.
Flickering occurs on the screen when the input signal is low resolution.
In fact, it looks like multiple vertical line noise.
conditions
Input signals: 640 x 480 60 p, 720 x 480 60 p (HDCP OFF)
Occurrence environment: An input signal is generated using a specific signal generator and occurs. HDMI Rx / Tx Used SN65DP159 for each interface.
Symptoms occurred when used with Rx side Retimer.
SN65DP159 Setting
Rx: Retimer mode (Across full range 250 Mbps to 6 Gbps)
Tx: Retimer mode or (Across full range 250 Mbps to 6 Gbps)
or
Automatically mode (Redriver to retimer cross over at 1.0 Gbps)
Input signals: 640 x 480 60 p, 720 x 480 60 p (HDCP OFF)
- It does not occur with HDCP ON.
- It does not occur even at 1024 x 768 60 p. (There is a threshold in VGA ~ XGA band)
A question
Why does it occur with low resolution Retimer mode?
Please tell me the cause and measures.
In 2017 input the VGA signal with TMDS 171. When used in Retimer mode,
Noise occurred on the screen. At this time, the register of the charge pump was not ON.
Does it occur with the same contents on SN65DP159?
Regarding the image of noise, I will send it if you can tell me the destination.
Thank you.