Part Number: DS90UB927QEVM
Hi team,
a customer of mine is looking into transmitting a LVDS display signal via a serialized FDP link. Back desalinized this signals should be displayed by a monitor (basically the setup in the pic below)
The LVDS signal is send out by an i.MX6 Host w.1280 x 800 pixel @ 60Hz.
The first approach was to serialize the signals wit the DS90UB927 and deserialize it back to LVDS with the DS90UB928. He picked up these two EVMs but is not able to get this setup running. If he connects the host and the monitor directly everything works.
Two option to support this come into my mind:
- we provide a step by step instruction how to set up this EVM combo
- can we recommend a different part / EVM what offer better plug & play characteristics?
Looking forward for you response - thank you very much!
Kind regards
Dierk Bronner