Part Number: TUSB1002A
Other Parts Discussed in Thread: TUSB1002, , HD3SS3202
Dear *,
1) Ti only has two IC that are re-driver only for USB3.1 Gen2
TUSB1002A and TUSB1002 is that correct?
2) Which one is better ->> TUSB1002A is a new device ?
3) DO we hate to put a re-driver on the UFP (Device side) ?
4) Where is the right place to put the redriver?
a) can we put the redriver between UPF device and HD3SS3202?
b) if we put the redriver between UFP and HD3SS3202 what is the recommended capacitor placement ?
c) do we need then to bias the HD3SS3202 and how?
Br,
D.