Part Number: TPS65987D
Other Parts Discussed in Thread: BQ25703
Hi.
I'm developing a power bank based on TIDA-01627 with TPS65987D controller.
As this application uses a BQ25703 charger that has to be intialized by the TPS65987D, my device will need some configuration data to be loaded in the external flash so it can execute the initialization sequences.
My doubt is: What is the recommended programmer for production in this type of application?
The configuration tool user manual mentions the aardvark programmer and FTDI programmer, I can see that the FTDI is integrated in the TPS65987EVM but its pins are not accessible for use with external devices.
As the aardvark programmer is pretty expensive, is there some cheaper EVM integrating the FT4232 that can be used with custom boards based on TPS65987D?
Thank you.