Part Number: TPS65987D
Hi
Could you please let me know your recommended device for following requirements?
USB port : TypeC UFP
Support PD detection (TypeC to TypeC, If DFP is not support PD, 5V/1.5A)
Support BC1.2 detection (typeA to TypeC)
Support port detection (A to C, C to C)
(want) support POWER IQ and QC detection
USB3.1
Power : In case of PD, 9V/3A(27W). in case of Non-PD, 5V/1.5A. (under 900mA is not accepted)
If it is connected 4.5W port, customer want alert signal.
Can we promote TPS65987D?
Could you please let me know your concerns? Also please tell me the reference design for this requirements.
Thanks
Muk