Part Number: LMH0346
Other Parts Discussed in Thread: LMH0344
Hi,
Context:
Our design is able to regenerated 4 distorted and Noisy HD-SDI video signal. In order to achieve this purpose, each channel use:
- 1 input connector (MCX 75Ω - RADIALL - R213424800);
- 1 Equalizer (TEXAS - LMH0344SQ/NOPB);
- 1 Recklocker (TEXAS - LMH0346SQ/NOPB);
- 1 driver (LMH0303SQ/NOPB);
- 1 output connector (MCX 75Ω - RADIALL - R213424800).
To deal with Build In Test requirement, we wanted to use the LMH0346's LOCKDETECT signal. For this reason, it is very important that this function is fully operationnal.
My problem:
When no input signal is present the LMH0346's Phase Loop Lock should be “unlock” and, consequently, LOCKDETECT signal should remain "Low". But in some channel, the LockDetect is not stable... On the unstable channel, the LOCKDETECT signal stay low during long period but get some oscillation (some High state occurs). Progressively, high state become longer and longer to finally remain High (about 1 minute after).
More information:
- Except LMH0346’s LOCKDETECT signal, the regenerated function works perfectly well.
- During my investigation, I use 3 different electronics boards. For each board, the problem occurs on different channels (Board#1 => Channel#1 Board#2 => Channel #1 Board#3 => Channel#3).
- I think the loop signal is very sensitive because the problem disappear just by touching the 56nF Loop Filter capacitor.
- I already study http://e2e.ti.com/support/interface/f/138/t/556985?tisearch=e2e-sitesearch&keymatch=LMH0346
My question:
- Have you already seen this kind of problem ?
- Could you help me to solve my trouble on the LMH0346's LOCKDETECT signal ?
Best regards,