Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
I just got a new board in which uses a DP83869HM as a simple media converter. SFP cage connected to fiber pins, copper Ethernet to RJ45 with integrated magnetics.
Configuration is just with straps, no SMI interface is connected.
The copper Ethernet connects up perfectly to all link partners I've tried But a logical connection through the SFP module to a different FMC does not connect. I didn't put some test points on this board to hook up the high speed differential probe so I'm not sure if the differential pairs to the SFP module are really working. I've done an SFP connection with other chips before so I'm pretty sure I did it correctly.
The other boards I've done with SFP modules did not use the LOS signal from the SFP module, the DP83869 DOES use this signal so I'm wondering if I did it right. I have the LOS connected to a 4.7K pull up resistor to 3.3V, it is connected to the SD pin (#24) on the DP83869. This done according to the diagram in the data sheet. But the data sheet never specifies the polarity or functionality of the SD pin. The LOS pin is a low value when the signal is good. The SD pin is not SDN, so I'm wondering if it is detecting good signal with a high value on the pin? I can't tell since the data sheet never says what the SD pin does.
I will attempt to solder in some test pins to look at the differential pairs going to the SFP module and see what they are doing.
Thanks,
John S.