This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: replicate mode : CSI port to port delay

Part Number: DS90UB954-Q1


what is the delay between CSI0 port and CSI1 port when replicate mode is used? The CSI ports output same data at the same timing? 

  • Hello Takuma-san,

    When using the 954 output replication mode, Lanes 0 and 1 + Clk0 will be CSI port 0, and lanes 2 and 3 + clk1 will be CSI port 1.
    Since both clk lanes will be sharing the same clock signal, and the same data on CSI port 0 is replicated on CSI port 1, both CSI clock outputs will be active and synchronous.