Part Number: TPS65981
Other Parts Discussed in Thread: , HD3SS460
Hello,
I'm trying to create a firmware for TPS65981 that enables a User Alternate Mode.
For this I tried to follow the recommendations in the document SLVA841 but did not succeed.
In order to make sure the hardware is ok, I’m using two evaluation boards TPS65981EVM from TI and connect them with a standard USB-C to USB-C cable.
How do I need to configure the TPS65981 so that when I connect the two TPS65981EVM with USB-C cable it configures the HD3SS460 for “4CH AM”? For this it is necessary that the lines AMSEL and EN would be high. Whatever I do this is never the case.
Could someone help me to figure out what I’m doing wrong. I could share the TPL project file I created.
Is there an example project somewhere available?
Thank you.
Regards,
Viktor