This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: DP83867

Guru 13485 points

Part Number: DP83867IR

Got below customer question:

We have on the card the DP83867IR set to RGMII mode with boot strap pin RX_DV/RX_CTRL pulled up by 2.49K to 1.8V, measured a voltage of 1.468V at reset so the device is set to mode 4

On the datasheet only modes 3 and 4 are permitted

The problem is that this mode sets the device to Manual Master/Slave Configuration – setting bit 12 on register 0x0009 to 1  - we read a value of 0x1300 from the register

Changing the boot strap to mode 0 – changing the pull up to pull down and getting 0.026V at reset the device mode is set to Disable Manual Master/Slave - we read a value of 0x0300 from the register

 

In the datasheet “Strap modes 1 and 2 are not applicable”

But the device will not work correctly in 1000Base-T if I set it to mode 4

 

In the datasheet the default value for this bit (reg 0x0009 bit 12) is 0 and setting the bit back to 0 solves the problem – but this is not in the standard Linux driver

 

Is this a problem with the datasheet? or there is another problem?