Part Number: TPS65981
Hello,
I am using a TPS65981 in a data DFP and power sink configuration (5V @ 1A and anywhere between 9V - 20V @ 3A). The chip is also connected to the external HD3SS460RHRT mux for USB3.0 and/or DisplayPort.
Problem
Currently the design does not support the following
- Flipping the cable
- DisplayPort doesn't work with version 4.03
- USB Doesn't work with version 4.03
The only thing, I think, of note within the 01.12.08 firmware release notes is number 4 on the bug fixes 'Fixed DPSourceSink Bit Status when the port is configured UFPD or DFPD on the Type C Connection' but I don't see how it can cause such a difference on the design.
Notes
Using the Application Customization I noticed different results with different versions of the configuration tool.
Here are the behaviors I've seen with Version 3.18 and Version 4.03
3.18
- Device is powered @ 20V
- USB Devices Work
- DisplayPort Does not go into DisplayPort Alternate Mode
- Works when cable is flipped
4.03
- Device is powered @ 20V
- USB Device Does Not Work
- TPS65981 Does not go into DisplayPort Alternate Mode
- Does not work when cable is flipped
When I switched the max voltage to 15V instead of 20V
3.18
- Device is powered @ 15V
- USB Devices Work
- DisplayPort Does go into DisplayPort Alternate Mode (DisplayPort isn't working but that may be an unrelated problem)
- Does not work when cable is flipped
4.03
- Device is powered @ 15V
- USB Device Does Not Work
- TPS65981 Does not go into DisplayPort Alternate Mode
- Does not work when cable is flipped
It seems as though I'm getting better results with the 3.18. Perhaps I'm doing something wrong.
I've attached a PDF of the relevant schematic pages, I followed the TPS65981EVM but I flipped the AMSEL and MX_CTL0_EN signals but I was able to fix them and add internal pull-up/pull-down resistors in the configuration tool. The schematic pages doesn't show this but R157, R158, R161 and R162 are unpopulated.
I've attached my configuration projects for both version of the configuration tool 3.18 and 4.03
I've also purchased a TotalPhase USB Power Delivery Analyzer and have captured logs of the 15V for both versions of the configuration. If you would like to view the logs you can get the tool Total Phase Data Center and open the logs