Part Number: TPS65981EVM
Dear Support,
when a new version of the doc will be available? the current one is not very good.
In particular: can you confirm the position of the switches as in 5.1.1.1 and 5.1.1.2 ??
Which is the default position for standard operation (no flashing etc etc)?
I am powering the board only from the microusb connector, I mean to use the FDTI bridge and I would like to run the "Notebook System" scenario.
Thanks
Francesco