This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Using PD controller without MCU

Part Number: TPS65987D

Hi TI,

My system need supply voltage 20Vdc from the adapter supports PD.

I don't need to change VBUS voltage (ex: 5V, 9V, 12V).

TPS65987D Can be used without MCU or memory?