This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/DS90UB960-Q1: Frame sync on 25 Mbps BC

Part Number: DS90UB960-Q1

Tool/software: TI-RTOS

Hi,

I have board with UB960 deserializer and I'm using IMX390 camera, with UB953 serializer. I want to use external PWM signal for frame sync. I'm able to get frame sync signal on UB953 GPIO when BC rate is 50 Mbps (0x58 = 0x5E).

But, due hardware issue currently I'm not able to use 50 Mbps BC, only 25 Mbps. When BC rate is 25 Mbps (0x58 = 0x5D), there is no frame sync signal on UB953 GPIO output.

Is there some limitation on using frame sync over FPD link when BC rate is 25 Mbps, or is there some additional configuration that needs to be done?

Best regards,

Stefan.