This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: How to select AC coupling capacitor

Part Number: DS90UB954-Q1

Hi team,

I have a question for AC coupling capacitor.

I will select the AC coupling capacitor with reference to the data sheet table. 228 Design Parameters.

In addition, 8.2.2 Detailed Design Procedure has the following description.

"For 2G operation or back channel frequency of ≤ 10 Mbps, the higher value AC-coupling capacitors 100 nF /47 nF are recommended."

In other words, does it mean that a small capacitor of 33 nF is recommended for fast communication at 4 Gbps?

We are considering the following usecase:

The forward channel datarate of 4Gbps and back channel frequency of 50Mbps

In this case, should we choose 33 nF / 15 nF?

Best regards,

Tomoaki Yoshida