Part Number: TPS65981
Hello,
I am following "application customization tool users guide" on Application Customization Tool 4.03 using the TPS65981EVM. In section 2.6, I am struggling finding the exact I2C address. It is unclear if that I2C is 7 bit or 8 bit. Also, From the schematic of the EVM DEBUG_CTL are also floating so it is either 7F or 4F. When I import the settings using the FTDI interface adapter I get that the import was successful no matter what address I use. It appears to be a false positive. Can you confirm the correct procedure on the TPS65981EVM.
-Jason