Part Number: TPS65981
Other Parts Discussed in Thread: TPS65982
Hello ,
I am building a custom board with the TPS65981 and I believe it is technically possible to drive two independent display controllers from my processor out of the TPS65981 and associated alternate mode mux/switches. My goal is to drive two independent displays with 60W of power on USB Type C, but in researching I found few examples of this configuration. I understand this is the TPS65981 forum but thought TI may have insight if this approach is possible and would better understand if there are any configuration options on power up that would need to be taken into account on the TPS65981.
-Jason