Part Number: DS90UB914A-Q1
Other Parts Discussed in Thread: DS90UB913A-Q1
Hi,
My customer is considering to use the DS90UB914A-Q1 and DS90UB913A-Q1.
They hope to control 913A's GPO by 914A's GPIO.
In the case of using GPIO0 pin, is following setting enough to use remote GPIO control?
DS90UB914A-Q1 setting
0X1D GPIO[1] and GPIO[0]Config
[0]GPIO Enable = 1 (enable)
[1]GPIO Direction = 1(input)
DS90UB913A-Q1 setting
0X1D GPIO[1] and GPIO[0]Configration
[0]GPIO Enable = 1 (enable)
[1]GPIO Direction = 0 (output)
[2]GPIO Remote Enable = 1 (Remote GPIO Enable)
Best Regards,
Kuramochi