Hi
I would like to input a clock signal with an amplitude deviation ± 3% to the IC using the spread spectrum function.
So please tell me the followings.
1. Although the amplitude deviation is ± 2.5% according to the specifications of the IC, what percentage of the amplitude deviation can be input as a performance?
2. Is there an IC that is pin compatible with the DS90UB925Q - O1 and can input with even greater amplitude deviation?