Part Number: TPS65986
Other Parts Discussed in Thread: TPS65982
Hello,
We have managed to capture a situation, where TPS65986 cannot load application code even though only single region is corrupted.
The differences are as follows: the first 4 bytes, i.e. Region Pointer (RPTR), from the region1 (high region) are corrupted (please see image in the file below for a quick glance).
To best of our knowledge, this should not prevent TPS65986 from loading region0 (low region). Could you please explain why region0 cannot load? Boot Flags register value is 0x00F490B8, which indicates, among other things, that there is a CRC error with region0. Could you please explain how this is possible?
--------------------
I checked the attached binaries and I can see your highlighted difference—that RPTR1 appears incorrect in the actual.bin. I also notice that the region headers in both bin files are 0xFF. I understand there is a worry about EC operation in this issue. I think one way to explain current PD operation is that there is a CRC issue with region 0 and region 1 fails to boot due to incorrect RPTR1.
Our recommendation is to ensure a valid full flash image with correct headers and pointers is set in device flash before EC based updates occur. Can you use the SPI programmer mentioned to perform a full update?
Regards,
Scott
------------------------
Thank you for your response! Please find our comments below.
You said: “I also notice that the region headers in both bin files are 0xFF.”
Considering the Figure 1 in [1], “Region 0 Pointer (RPTR0)” and “Region 0 Offset (AOFF0)” should be OK in both files.
The documentation [2] also says:
“Each header contains a region pointer (RPTR) that holds the address of the physical location in memory where the low-region application code resides. Each also contains an application-code offset (AOFF) that contains the physical offset inside the region where the TPS65982 application code resides”
Based on the image and the textual description, we believe region0 should be OK. Could you please elaborate: is there something else that should be included in a region header? Perhaps something between a region pointer and region offset? TI Application Customization Tool does not seem to generate anything but 0xFF between those values.
You said: “I think one way to explain current PD operation is that there is a CRC issue with region 0 and region 1 fails to boot due to incorrect RPTR1.”
As for the "there is a CRC issue with region 0", that was our observation as well, but could you please elaborate why region 0 has a CRC issue even though the contents should be OK?
As for the "region 1 fails to boot due to incorrect RPTR1", this is clear.
You said: “Our recommendation is to ensure a valid full flash image with correct headers and pointers is set in device flash before EC based updates occur.”
At the moment, we are considering to remove region header update (write between absolute addresses 0x0000 – 0x1FFF) as it is already written before any possible field updates.
You said: “Can you use the SPI programmer mentioned to perform a full update?“
Yes. That is what we do during manufacturing.