This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: Two TUSB8041s case, USB_VBUS

Genius 17355 points
Part Number: TUSB8041

Hello,

 

When two TUSB8041s are connected as the below figure, I would like to confirm what signal should be connected to USB_VBUS pin of the 2nd TUSB.


 

Should PWRCTLx/BATENx be connected to  USB_VBUS pin of the 2nd TUSB?

Or should 3.3V or 1.1V hub power be connected to it? If so, what resistance value should be used in resistor divider?

 

Regards,

Oba