This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: USB2.0 can connect, but USB3.0 can't connect

Part Number: TUSB9261

Hi Team,

My Customer Use TUSB9261 with FW(TUSB926x_FW_v1.06_SATA_NO_POLARITY_SWAP.bin) for USB 3.0 to SATA HDD.
Problems encountered as follows:
1,USB3.0 Cannot Successful communication when DP,DM is not connected.
2,USB3.0 Can Successful communication when DP,DM is connected.Disconnecting DP,DM does not affect when it is already communicating normally.
USB3.0 communication does not require connection to DP,DM Normally.
So,We think that the FW uses the DP,DM in the communication handshake.If the DP,DM is not connected, the handshake cannot be performed.
Our PCB has been completed.Can We solve this problem by modifying the software( Firmware)?Thanks!!