Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65CML100: power consumption

Part Number: SN65CML100

Team, my customer has a question:

I am not able to get power consumed by sn65cml100 when operating at

  1. 1. speed of 1.5Gbps,
  2. 2. LVDS input and
  3. 3. CML output

by going through its data sheet.

Is the Icc of max of 12mA  at 85C, correct?

It consumes only like 40mW at that speed?

Thanks

Viktorija